Article #: KA-03648
Published: 11th Jan 2024
Last reviewed: 15th Aug 2024
Unable to ping or SNMP poll G5/G6 PDU
Contents
Introduction
This article explains steps to take if you are unable to communicate with a G5 or G6 PDU across your network. It outlines 2 scenarios, one where the unit is not pingable and the other where the unit is pingable, but there is no SNMP communication.
Purpose
If a Panduit G5 or G6 PDU becomes unreachable, follow these steps to attempt to recover. If these steps fail to recover the unit, please contact systemsupport@panduit.com to raise a support caseRequirements
- Good networking knowledge- SNMP Knowledge
Procedure
PDU is not pingable
- Is the physical connection to the PDU network port good?
- Is the PDU controller unit powered up? Do you see anything on the display?
- NO – check power to the PDU
- Try removing the controller from the PDU and check the ribbon cable for kinks and then reseat the connection to see if the controller come back on.
- Reset the controller by pressing the ‘reset’ button on the from panel for less than 8 seconds – this initiates a ‘soft’ reset of the controller, retaining all configuration data.
- Does the IP address being pinged match that shown on the PDU OLED screen (under Setup>Network>IP Address)
- Check for duplicate IP addresses on the network by removing the network cable from the PDU and checking if that IP now responds to a 'ping' command
- Is the PDU running latest firmware? If not, upgrade using the BCT tool or Web GUI (latest firmware versions are available from https://www.panduit.com/en/support/download-center/power-distribution-units.html)
- Are there any daisy chained PDUs connected? Remove daisy chained units, reset master and retry ping
- Are there any sensors connected? Remove, reset and then retest.
- Connect to the network port of the PDU using a directly connected laptop on the same network address range (Full instructions are in Appendix G of the G5 User guide downloadable here https://www.panduit.com/en/support/download-center/power-distribution-units.html)
- Are you able to communicate with the unit using the serial port? (see the G5 user guide Appendix H, downloadable from the link above.
- If none of the above is successful, Perform a factory reset on the PDU by holding down the ‘reset’ button for >20 seconds. Remove/re-apply power to PDU. NOTE – this will erase all configuration and reset to factory defaults
- If the unit still will not communicate, raise a Technical support ticket by emailing systemsupport@panduit.com.
No SNMP communication
If the PDU is pingable across the network, but your SNMP monitoring platform is unable to poll/receive traps from the unit, please check the following:- Ensure that network ports 161 and 162 are fully open between the PDU and monitoring platform, ensure that all network devices have these ports open.
- Ensure that the PDU is configured correctly – details are contained in the G5 User manual under Section 3 – available from here https://www.panduit.com/en/support/download-center/power-distribution-units.html
Panduit.com SystemsSupport@panduit.com 1-866-721-5302 Article: KA-03648